X5-Applications
| ||||||
BATCHBatch is an application to allow automation of batching, manual additions and production steps.
| ||||||
Batch [X5-Firm]This file is a ready to use application for a PR1713-X5 device. NOTE: Your need => FlashIt!32 to load the file into the device Batch [X5-Firm] 03.01.08/03.40.09
see archive for older versions | ||||||
Batch [Customizing Kit]This kit contains all files needed to translate the Batch application or to add print labels. Batch [Customizing Kit] 03.01.08
see archive for older versions | ||||||
BulkBULK is an application software to realize circuit scales for loading and unloading of ships, trains and trucks. | ||||||
Bulk [X5-Firm]This file is a ready to use application for a PR1713-X5-X6 device. NOTE: Your need => FlashIt!32 to load the file into the device Bulk [X5-Firm] 03.00.11/03.40.09
see archive for older versions | ||||||
Bulk [Customizing Kit]NOTE! Firmware 2.20.7 and Bios 2.12 is recommended for this Customizing kit Bulk [Customizing Kit] 03.00.11
see archive for older versions | ||||||
FILLFILL is an application to fill liquids in drums, bins, containers etc.
| ||||||
FillController [X5-Firm]This file is a ready to use application for a PR1713-X5 device. NOTE: Your need => FlashIt!32 to load the file into the device FillController [X5-Firm] 03.00.02/03.40.09
see archive for older versions | ||||||
FillController [Customizing Kit]This kit contains all files needed to translate the FillController application or to add print labels. FillController [Customizing Kit] 03.00.02
see archive for older versions | ||||||
FLOWThis software controls the product flow using a gravimetric method for loss in weight of filling applications.
| ||||||
FlowController [X5-Firm]This file is a ready to use application for a PR1713-X5 device. NOTE: You need => FlashIt!32 to load the file into the device FlowController [X5-Firm] 03.02.05/03.40.09
see archive for older versions | ||||||
FlowController [Customizing Kit]This kit contains all files needed to translate the FlowController application or to add print labels. FlowController [Customizing Kit] 03.02.05
see archive for older versions | ||||||
IBCIBC is an application for an 'Intermediate Bulk Container'-station.
| ||||||
IBC [X5-Firm]This file is a ready to use application for a PR1713-X5 device. NOTE: Your need => FlashIt!32 to load the file into the device IBC [X5-Firm] 03.01.03/03.40.09
see archive for older versions | ||||||
IBC [Customizing Kit]This kit contains all files needed to translate the IBC application or to add print labels. IBC [Customizing Kit] 03.01.03
see archive for older versions | ||||||
LOGLOG is an application to weigh and register incoming and outgoing material.
| ||||||
LOG [X5-Firm]This file is a ready to use application for a PR1713-X5 device. NOTE: Your need => FlashIt!32 to load the file into the device LOG [X5-Firm] 02.22.00/03.14.02
see archive for older versions | ||||||
LOG [Customizing Kit]This kit contains all files needed to translate the LOG application or to add print labels. LOG [Customizing Kit] 02.22.00
see archive for older versions | ||||||
MIXMixController is an application to use PR1713/X5/X6 for manual and semi automatic dosing recipes. | ||||||
MixController [X5-Firm]This file is a ready to use application for a PR1713/X5/X6 device. NOTE: Your need => FlashIt!32 to load the file into the device MixController [X5-Firm] 01.00.04/03.40.09
see archive for older versions | ||||||
MixController [Customizing Kit]This kit contains all files needed to translate the MixController application or to add print labels. MixController [Customizing Kit] 01.00.04
see archive for older versions | ||||||
PHASEPhaseController is an application to use PR1713/X4/X5/X6 as
| ||||||
PhaseController [X5-Firm]This file is a ready to use application for a PR1713/X5/X6 device. NOTE: Your need => FlashIt!32 to load the file into the device. PhaseController [X5-Firm] 01.10.07/03.40.09
see archive for older versions | ||||||
PhaseController [Customizing Kit]This kit contains all files needed to translate the PhaseController application. PhaseController [Customizing Kit] 01.10.07
see archive for older versions | ||||||
PROProController is an application to use PR1713/X4/X5/X6 as
| ||||||
ProController [X5-Firm]This file is a ready to use application for a PR1713/X5/X6 device. NOTE: Your need => FlashIt!32 to load the file into the device ProController [X5-Firm] 03.00.02/03.40.09
see archive for older versions | ||||||
ProController [Customizing Kit]This kit contains all files needed to translate the ProController application or to add print labels. ProController [Customizing Kit] 03.00.02
see archive for older versions | ||||||
TRUCK-X5Stand alone weighbridge application.
| ||||||
TruckLine [X5-Firm]This file is a ready to use application for a PR1713-X5 device. NOTE: Your need => FlashIt!32 to load the file into the device TruckLine [X5-Firm] 04.00.02/03.40.09
see archive for older versions | ||||||
TruckLine [Customizing Kit]This kit contains all files needed to translate the TruckLine application or to add print labels. TruckLine [Customizing Kit] 04.00.02
see archive for older versions | ||||||
| © Sartorius Mechatronics, 2010 | ||||||