| | | |
Archive of all X5-Applications downloads This is the complete archive of X5-Applications available for download from Sartorius Mechatronics. It is provided as convenience for customers, who need to use specific versions of a given software. For new development we strongly recommend to use the current releases found on List of latest X5-Applications downloads. | | |
| | | |
| | |
| | | |
BATCH | | |
| | | |
| | |
| | | |
Batch [X5-Firm] - Released with firmware rel 03.40.09
- Released with firmware rel 03.40.08
- Released with firmware rel 03.40.07
- Fixed start functionality via fieldbus and OPC.
- Fixed print error with character “$A0”
- Included new version of library
- Released with firmware rel 03.40.023
- Released with firmware rel 03.40.02.
- Released with firmware rel 03.30.08.
- Fixed batch mode A1
- Released with firmware rel 03.30.05.
- Released with firmware rel 03.30.02.
- Released with firmware rel 03.30.00.
- Fixed EW-Command LR (READ), selected report will be deleted after read.
- Fixed labels with actual version of NLE
- Released with firmware rel 03.16.05
- Released with firmware rel 03.16.05
- Repair: the I/O of PR1713/13 can now be assigned (SETUP->CONFIG)
- Repair: String 'PR1740' changed to 'PR8400'.
- Repair: changed error text 'analog error' to 'invalid weight'
- Repair: Remote start of recipes: unit of set point is now lb when unit of weighing point is lb.
- Application is build with PR1750 version 3.00.00 !!
- Repair: Remote start of recipes is now possible with ProBatch+.
- Repair: Softkey 'Abort' is now enabled for batch mode D1 and D2 instead of 'Return'
- Released with firmware rel 03.14.02
- Updated to Batch 03.00.00
- Released with firmware rel 2.20.07
- Updated to Batch 2.20.01
- Released with firmware rel 2.20.5
- Released with firmware rel 2.20.3
- Released with firmware rel 2.20.2
- Released with firmware rel 2.20.1
- Released with firmware rel 2.20
- new display modes during recipe status display
- new protection function: prohibit operator to enter any component, recipe or clear consumption or production
- binary coded recipe start via digital inputs
Changes in Batch 02.02: - Added : preparation for free configurable weighing points (available with Firmware 2.10...)
- Added : spm %MB317 enables FSD-check for dosing phases
| | |
| | | |
| | |
| | | |
Batch [Customizing Kit] - Fixed start functionality via fieldbus and OPC.
- Fixed print error with character “$A0”
- Included new version of library
- Fixed batch mode A1
- Released with firmware rel 03.30.05.
- Fixed EW-Command LR (READ), selected report will be deleted after read.
- Fixed labels with actual version of NLE
- Repair: the I/O of PR1713/13 can now be assigned (SETUP->CONFIG)
- Repair: String 'PR1740' changed to 'PR8400'.
- Repair: changed error text 'analog error' to 'invalid weight'
- Repair: Fieldbus functions of application
NOTE! Firmware 2.20 and Bios 2.12 is recommended for this Customizing kit Please download => PR1713-X5-Firmware 2.20 to get all supplemental files - This is the first version available.
| | |
| | | |
| | |
| | | |
Bulk | | |
| | | |
| | |
| | | |
Bulk [X5-Firm] - Released with firmware rel 03.40.09
- Released with firmware rel 03.40.08
- Released with firmware rel 03.40.07
- Released with firmware rel 03.40.03
- Released with firmware rel 03.40.02
- Released with firmware rel 03.30.08
- Migrated to 1750-60
- Added standard fieldbus interface - scale only
- Power up failure after power fail fixed. Reactivating single conversion if power fail recognized, reset power fail flag then
- Add ixEnSumClear on %IX2.3 as an hardware enable for sumclear commands
- Add clearing sum counters to operator level Operator may enter 'Manual', 'Totals' if ixEnSumClear is active. Then he can select which counters/totals to delete and whether he wants a printout before deletion. If printout is selected, an actual date header will be printed. Then the same for device production total - which is in db_sys and earom
- Material table print includes totals with names C1, C2, C3
- Released with firmware rel 03.30.06
- Migrated to 1750-60
- Added standard fieldbus interface - scale only
- Power up failure after power fail fixed. Reactivating single conversion if power fail recognized, reset power fail flag then
- Add ixEnSumClear on %IX2.3 as an hardware enable for sum clear commands
- Add clearing sum counters to operator level Operator may enter 'Manual', 'Totals' if ixEnSumClear is active. Then he can select which counters/totals to delete and whether he wants a printout before deletion. If printout is selected, an actual date header will be printed. Then the same for device production total - which is in db_sys and earom
- Material table print includes totals with names C1, C2, C3
- Released with firmware rel 03.30.06
- Application is built with PR1750-50 version 3.00.xx !!
| | |
| | | |
| | |
| | | |
Bulk [Customizing Kit] - First Release for PR1750-50
- First Release for PR1750-50
- NOTE! Firmware 2.20.7 and Bios 2.12 is recommended for this Customizing kit
| | |
| | | |
| | |
| | | |
FILL | | |
| | | |
| | |
| | | |
FillController [X5-Firm] - Released with firmware rel 03.40.09
- Released with firmware rel 03.40.08
- Released with firmware rel 03.40.07
- Released with firmware rel 03.40.03
- Released with firmware rel 03.40.02
- Released with firmware rel 03.30.08
- Released with firmware rel 03.30.05
- Released with firmware rel 03.30.02
- Released with firmware rel 03.30.00
- Fixed labels with actual version of NLE
- Released with firmware rel 03.16.07
- Released with firmware rel 03.16.05
- fieldbus for application reactivated
- fieldbus for application reactivated
Updated to Firmware 2.20.07 This is the first version available. | | |
| | | |
| | |
| | | |
FillController [Customizing Kit] - Fixed labels with actual version of NLE
- fieldbus for application reactivated
This is the first version available. | | |
| | | |
| | |
| | | |
FLOW | | |
| | | |
| | |
| | | |
FlowController [X5-Firm] - Changed: Added new config parameter 'Auto start at 2mA'. Controls automatic start of process on configuration external setpoint and 4 – 20mA
- Released with firmware rel 03.40.09
- Fixed: If configured as flowmeter (loop controller off) and 4..20mA output the output would permanently be 0mA
- Fixed problem after powerfail, restart filter
- Released with firmware rel 03.40.08
- Released with firmware rel 03.40.07
- Released with firmware rel 03.40.03
- Released with firmware rel 03.40.02
- Released with firmware rel 03.30.05
- Fixed problem after powerfail, restart filter
- Released with firmware rel 03.30.06
- Released with firmware rel 03.30.02
- Released with firmware rel 03.30.00
- Changed: Overload during refill is allowed
- Fixed: Check refill min and max only if automatic refill is activated
- Released with firmware rel 03.16.07
- Released with firmware rel 03.16.05
- Changed: If starting by field bus the flow set point is taken from last value receive from field bus, not from materials table.
- Changed message: Loop controller 'flow set point source' mentions now 'field bus' together with 'local'. Function not changed.
- Fixed: Device configuration for serial remote output.
- Fixed: Gross limit bit for field bus is now bit 45.
- Fixed: Start table can now be measured with filter < 0.5 Hz.
- Added: Program 'Test' to check weighing point electronics.
- New specification:
- Flow set point via operating, field bus, serial line and analogue input
- 3 modes: measure flow rate, control flow and cascaded controller (optional)
- Simple dosing
- Up to 2 analogue outputs cards
- Extended configuration
- Extended refill before starting
- Simulation, configured in 'Config'
- The material database is incompatible with older releases
- Fixed: Digital IO
- Fixed: Field bus interface is activated now.
- Fixed: Display of flow, total, ... on weight display, requires Firmware >= 2.20.
| | |
| | | |
| | |
| | | |
FlowController [Customizing Kit] - Changed: Added new config parameter 'Auto start at 2mA'. Controls automatic start of process on configuration external setpoint and 4 - 20mA
- Fixed: If configured as flowmeter (loop controller off) and 4..20mA output the output would permanently be 0mA
- Fixed problem after powerfail, restart filter
- Fixed problem after powerfail, restart filter
- Changed: Overload during refill is allowed
- Fixed: Check refill min and max only if automatic refill is activated
- Changed: If starting by field bus the flow set point is taken from last value receive from field bus, not from materials table.
- Changed message: Loop controller 'flow set point source' mentions now 'field bus' together with 'local'. Function not changed.
- Fixed: Device configuration for serial remote output.
- Fixed: Gross limit bit for field bus is now bit 45.
- Fixed: Start table can now be measured with filter < 0.5 Hz.
- Added: Program 'Test' to check weighing point electronics.
- New specification: Requires Firmware >= 3.12.
- Flow set point via operating, field bus, serial line and analogue input
- 3 modes: measure flow rate, control flow and cascaded controller (optional)
- Simple dosing
- Up to 2 analogue outputs cards
- Extended configuration
- Extended refill before starting
- Simulation, configured in 'Config'
- The material database is incompatible with older releases
- Fixed: Digital IO
- Fixed: Field bus interface is activated now.
- Fixed: Display of flow, total, ... on weight display, requires Firmware >= 2.20.
- Fixed: Process can be restarted after power failed as described.
- Changed: Adapted to firmware >= 2.20.
- Changed: Adapted to firmware > 2.10.2.
- Base Release: Requires Firmware 2.10 or better !
| | |
| | | |
| | |
| | | |
IBC | | |
| | | |
| | |
| | | |
IBC [X5-Firm] - Released with firmware rel 03.40.09
- Released with firmware rel 03.40.08
- Released with firmware rel 03.40.07
- Released with firmware rel 03.40.03
- Released with firmware rel 03.40.02
- Released with firmware rel 03.30.08
- Released with firmware rel 03.30.05
- Released with firmware rel 03.30.02
- Released with firmware rel 03.30.00
- Fixed labels with actual version of NLE
- Released with firmware rel 03.16.07
- Fixed: Customer defined report texts are available for NLE
- Fixed: Setting inputs 'Stop' and 'Abort' at the same time --> hang up #1492
- Fixed: Slot 3 is not configurable in application
- Released with firmware rel 03.16.05
- Compiled with PR1750 version 3.00.00
- changed error text 'analog error' to 'invalid weight'
- Fieldbus for application reactivated
- tare with given fixtare from bin-table and batch mode B2: tare is set now
| | |
| | | |
| | |
| | | |
IBC [Customizing Kit] - Fixed labels with actual version of NLE
- Fixed: Customer defined report texts are available for NLE
- Fixed: Setting inputs 'Stop' and 'Abort' at the same time --> hang up #1492
- Fixed: Slot 3 is not configurable in application
- Compiled with PR1750 version 3.00.00
- changed error text 'analog error' to 'invalid weight'
- Fieldbus for application reactivated
- tare with given fixtare from bin-table and batch mode B2: tare is set now
| | |
| | | |
| | |
| | | |
LOG | | |
| | | |
| | |
| | | |
LOG [X5-Firm] - fieldbus reactivated for application
- Updated to Firmware 2.20.07
- This is the first version available.
| | |
| | | |
| | |
| | | |
LOG [Customizing Kit] - fieldbus reactivated for application
- This is the first version available.
| | |
| | | |
| | |
| | | |
MIX | | |
| | | |
| | |
| | | |
MixController [X5-Firm] - Released with firmware rel 03.40.09
- Released with firmware rel 03.40.08
- Released with firmware rel 03.40.07
- Released with firmware rel 03.40.03
- Released with firmware rel 03.40.02
- Released with firmware rel 03.30.08
- Released with firmware rel 03.30.05
- Released with firmware rel 03.30.02
- Released with firmware rel 03.30.00
- Fixed labels with actual version of NLE
- Released with firmware rel 03.16.07
- Changed: Edit order is now not checking setpoint against FSD.
- Released with firmware rel 03.16.05
| | |
| | | |
| | |
| | | |
MixController [Customizing Kit] - Fixed labels with actual version of NLE
Fixed: Option analogue IO in slot 3 is possible now. Fixed: Set point is correct calculated if material used 'Dialog'. Fixed: Kit contains the label files now. | | |
| | | |
| | |
| | | |
PHASE | | |
| | | |
| | |
| | | |
PhaseController [X5-Firm] - Released with firmware rel 03.40.09
- Released with firmware rel 03.40.08
- Released with firmware rel 03.40.07
- Released with firmware rel 03.40.03
- Released with firmware rel 03.40.02
- Fixed: ProBatch+ problem during discharge sends weight error
- Fixed: Component D4_Dialog is directly approved, message never shown
- Released with firmware rel 03.30.08
- Released with firmware rel 03.30.05
- Fixed: Recipe start and parameter "Production with recipe total" is activated in ProBatch+.
- Fixed: SPM set/reset from different weighing points.
- Released with firmware rel 03.30.02
- SPMinBit and SPMinTareBit are now triggered on rising edge (D1, D2).
- Released with firmware rel 03.30.00
- Fixed: pi.oActual value is set one state earlier for ProBatch+ (D2).
- Released with firmware rel 03.20.00
- Released with firmware rel 03.16.07
- Fixed: Analog Output 4..20mA, offset error
- Released with firmware rel 03.16.05
- Released with firmware rel 03.16.03
- Released with firmware rel 03.16.01
- Manual phase ( D1, D2 ): the optional dialog is done before dosing any material.
- Operating of D1 in case of tolerance alarm is now similar to automatic dosing ( B1, ... ). 'continue' is the the same on PC and on the controller. 'abort' on PC does not have the function of 'accept' on the controller and aborts the phase ( line marked: '*' ).
- Tolerance alarm, flow warning and phase held signals are now in virtual SPM:
Bit 16: tolerance alarm WP-A 17: flow warning WP-A 18: phase in held state WP-A Bit 24: tolerance alarm WP-B 25: flow warning WP-B 26: phase in held state WP-B - SPMout for the timer phase ( D3 ) is set again again after restarting a stopped phase.
- This is the first version available
| | |
| | | |
| | |
| | | |
PhaseController [Customizing Kit] - Fixed: ProBatch+ problem during discharge sends weight error
- Fixed: Component D4_Dialog is directly approved, message never shown
- Fixed: Recipe start and parameter "Production with recipe total" is activated in ProBatch+.
- Fixed: SPM set/reset from different weighing points.
- SPMinBit and SPMinTareBit are now triggered on rising edge (D1, D2).
- Fixed: pi.oActual value is set one state earlier for ProBatch+ (D2).
- Fixed: Analog Output 4..20mA, offset error
- Manual phase ( D1, D2 ): the optional dialog is done before dosing any material.
- Operating of D1 in case of tolerance alarm is now similar to automatic dosing ( B1, ... ). 'continue' is the the same on PC and on the controller. 'abort' on PC does not have the function of 'accept' on the controller and aborts the phase ( line marked: '*' ).
- Tolerance alarm, flow warning and phase held signals are now in virtual SPM:
Bit 16: tolerance alarm WP-A 17: flow warning WP-A 18: phase in held state WP-A Bit 24: tolerance alarm WP-B 25: flow warning WP-B 26: phase in held state WP-B - SPMout for the timer phase ( D3 ) is set again again after restarting a stopped phase.
- This is the first version available
| | |
| | | |
| | |
| | | |
PRO | | |
| | | |
| | |
| | | |
ProController [X5-Firm] - Released with firmware rel 03.40.09
- Released with firmware rel 03.40.08
- Released with firmware rel 03.40.07
- Fixed problem during test scale function
- Released with firmware rel 03.40.03
- Released with firmware rel 03.40.02
- Released with firmware rel 03.30.08
- Released with firmware rel 03.30.05
- Released with firmware rel 03.30.02
- Released with firmware rel 03.30.00
- Attention: Based on Pro Controller 02.12.04 will only work with firmware version 03.20.00 or newer
- Changed: New implementation of the alibi memory
- Changed: EWCOM WGA, return weight value is now like PR1613
- Released with firmware rel 03.20.00
- Outputs 7 + 7 ale available now via MX 1222 and MX 1223
- Released with firmware rel 03.16.07
- Released with firmware rel 03.16.05
- Fixed: Analogtest fails if Error 2
- Fixed: Parameters in CONFIG are modified by 'overwrite' now
- Changed: Clock is now also checked while running program START
- Fixed: Text 'Limit' corrected
- Changed: Text 'Build in' replaced by 'Builtin RS232'
- Changed: Current configuration data is restored immediately if 'Store data ?' is 'No'
- Fixed: BCD digital output configuration is not longer reset if output 1 is 'none'
- Label template prepared for NiceLabelExpress 2.8
- Fieldbus in slot 4 activated now
- Updated to Firmware 2.20.07
- This is the first version available.
| | |
| | | |
| | |
| | | |
ProController [Customizing Kit] - Fixed problem during test scale function
- Attention: Based on Pro Controller 02.12.04 will only work with firmware version 03.20.00 or newer
- Changed: New implementation of the alibi memory
- Changed: EWCOM WGA, return weight value is now like PR1613
- Outputs 7 + 7 ale available now via MX 1222 and MX 1223
This Customizing Kit requires a Firmware 3.12 or better. - Fixed: Parameters in CONFIG are modified by 'overwrite' now
- Changed: Clock is now also checked while running program START
- Fixed: Text 'Limit' corrected
- Changed: Text 'Build in' replaced by 'Builtin RS232'
- Changed: Current configuration data is restored imediately if 'Store data ?' is 'No'
- Fixed: BCD digital output configuration is not longer reset if output 1 is 'none'
This Customizing Kit requires a Firmware 3.12 or better. - Label template prepared for NiceLabelExpress 2.8
- Fieldbus in slot 4 activated now
- Adapted to support X4 hardware.
- BCD output follows display now is configured.
- Analogue output switches to Gross if not tared and configured.
- Old EWCOM commands "WGA" and "WSA" are working correct now.
- Specific messages if problems with printing.
- Fixtare via SPM added
This is the first version available. | | |
| | | |
| | |
| | | |
TRUCK-X5 | | |
| | | |
| | |
| | | |
TruckLine [X5-Firm] - released with firmware 3.40.09
- released with firmware 3.40.08
- released with firmware 3.40.07
- released with firmware 3.40.03
- released with firmware 3.40.02
- Fixed: Get weight function in dosing mode
- Released with firmware rel 03.30.08
- Released with firmware rel 03.30.05
- Released with firmware rel 03.30.02
- Fixed read weight without alibi license
- Released with firmware rel 03.30.00
- Attention: Based on TruckLine 03.04.03 will only work firmware version 03.20.00 or newer
- Changed: New implementation of the alibi memory
- Released with firmware rel 03.16.07
- Fixed: PLC start not until init done #1517.
- New: Two new parameter for the configuration.
- Fixed: Configuration hangs up if CAL-switcher is locked
- Released with firmware rel 03.16.05
- Fixed: Configuration of printing the log and statistics on a 2nd / 3rd printer
New specification: - Dosing added: automatic, manual, registration ( requires license PR1713/32 )
- Density for set point and net weight added
- Temporary customer addresses
- Report database added - to be used with AccessIt!
- Order number stored as string ( no LINT ) to be used with AccessIt!
- Extra ticket for dosing
- Simple configuration for ticket layout
- Configuration for input, output and limits
- Fieldbus interface added
- 1 variable + 2 fixed comment lines to be reported
- Prompt text variable for variables comment line is a configuration parameter
- Preparation for second code page on display
- Tare weighing books net now only depending on keyboard input
Restrictions: - Databases are not compatible with former versions due to many new features
- Released with firmware rel 2.20.3
| | |
| | | |
| | |
| | | |
TruckLine [Customizing Kit] - Fixed get weight function in dosing mode
- Fixed read weight without alibi license
- Attention: Based on TruckLine 03.04.03 will only work firmware version 03.20.00 or newer
- Changed: New implementation of the alibi memory
- Fixed: PLC start not until init done #1517.
- New: Two new parameter for the configuration.
- Fixed: Configuration hangs up if CAL-switcher is locked
- Fixed: Configuration of printing the log and statistics on a 2nd / 3rd printer
New specification: - Dosing added: automatic, manual, registration ( requires license PR1713/32 )
- Density for set point and net weight added
- Temporary customer addresses
- Report database added - to be used with AccessIt!
- Order number stored as string ( no LINT ) to be used with AccessIt!
- Extra ticket for dosing
- Simple configuration for ticket layout
- Configuration for input, output and limits
- Fieldbus interface added
- 1 variable + 2 fixed comment lines to be reported
- Prompt text variable for variables comment line is a configuration parameter
- Preparation for second code page on display
- Tare weighing books net now only depending on keyboard input
Restrictions: - Databases are not compatible with former versions due to many new features
| | |
| | | |
| | |
| | | |
| | | |
| | |
| | |
| © Sartorius Mechatronics, 2010 | | |
| | |
| | |
| | |