PR1713-X5-Firm Add: GET_WEIGHT(ZERO_SET) Add: method to pass standstill and error for user-wp from application Fix: CCLink reads a wrong number of input bytes Fix: Received characters got lost by a race-condition in DEV_KEYKEY when timeout occured while received character was processed. - Fixed: Do not show DHCP option for PR1713 X5
- Fixed: rounding for NET10-Weights
- Change: added a timeout for checking the correct function of a fieldbus card
- Change: send always the unit to the remotedisplay
- Change: send always the number of digits behind the decimalpoint to the remotedisplay
- Fixed: Profibus and Devicenet cards are not correct initialized
- Fixed: Profibus and Devicenet cards are not correct initialized
- Fixed: the ethernet card PR1713/14 was not detected during power up
- don't send special command (P) to remotedisplay
- New implementation of the alibi memory (needs a new version of 1750)
- Fixed : reading the BAT_REPO_HEADER table via OPC fails after running a new batch.
Only the last report was visible. - Fixed : #1515 calculation in hysteresis correction
- Fixed : #1517 memory corruption on index-errors in flashed programs
- Fixed : Setup xBPI-Scale : Show current parameter settings even if parameter change is disabled
- Fixed : On specific conditions Variable-Debug in PR1750 resulted in KUW_BAD_SIZE error
This Firmware Version requires Applications compiled with PR1750 Rel 2.32 or better. Changes from Rel 3.16.4 to 3.16.5 - Fixed : Overload in multirange used wrong limits
- Fixed : #0001328 reading scale and application via fieldbus intermixed data if two or more plc-task used in application
- Fixed : #0001322 Always reset fieldbus-slave on cpu-reset (bios-03.16.06)
- Fixed : Mixing W&M-WP with none-W&M-WP didn't show wgt-unit in display (wrong hardwarecode in bios)
Changes from Rel 3.16.3 to 3.16.4 - Fixed : Display for large values on poly-range xBPI-Scales
- Fixed : Diff was calculated for wrong setpoint in B8
Changes from Rel 3.16.2 to 3.16.3 - Changed : Default for xBPI taring now local
- New protocoll 2-wire in serial setup
- Fixed : Diff was calculated for wrong setpoint in B4,B5
This Firmware Version requires Applications compiled with PR1750 Rel 2.32 or better. - Fixed : Diff was calculated for wrong setpoint in B4,B5
This Firmware Version requires Applications compiled with PR1750 Rel 2.32 or better. This Firmware Version requires Applications compiled with PR1750 Rel 2.32 or better. - Fixed : checking for I/O-Configuration always returned 'BadConf'
- Fixed : Interrupts during powerfail were not disabled
- Fixed : If a batch was active on powerfail the coarse,fine signals are set for 2 sec on power up
- Fixed : Calculation of FSD for A+B Scale with OIML enabled
- Fixed : ReadValue.Byte6.Bit6 and WriteCommand 121dez were corrupted (since Rel 2.10)
- Fixed : On Terminal Weighingpoints WP 'D' could be selected followed by a crash
- Change : Factory licenses are copied to earom during coldstart
- Added : Support of PR5710/12 in X6
- Change : Factory licenses are copied to earom during coldstart
- Added : Support of PR5710/12 in X6
- Fixed : JBUS did crash when master sends a new request while slave sends an answer
- Fixed : Analoginput component sends an incorrect report
- Fixed : select a record via number in second display line missed the first digit
- Fixed : the OPTION statement will return PR1721 if the new fieldbuscards (HMS) are inserted.
- Fixed : Set and remove breakpoints from PR1740 will crash.
- Fixed : accept a cancel from Recoverit! during up/download. added timeout for receiving, task finish after 1 minute of inactive communication
- Fixed : DSP_INPUT on string crashed, when content of last string result was longer than the edited string variable
- Change : DSP_INPUT on TimeOfDay and DateAndTime value check fixed
- Fixed : STRING_TO_DATE on 1980..1999 return bad date
- Fixed : EQUAL of struct nearly always returned false, if struct had arrays of BOOL inside.
- Change : DBASE now ignores fraction of seconds in TIME_OF_DAY and DATE_AND_TIME to be more compatible with PC databases
NOTE! this Firmware is intended to be used with X5 application customizing kits rel 2.12 only Please use => Rel 2.02.4 for application customizing kits Rel 2.02. - Added : Free assignment of weighingpoints
- Added : Support of xBPI-Scales
- Added : Support of PR1721/1x modules
- See PR1713-X5-Firm History.txt for a complete list
- Added : Display-Segment test on power up
- Added : W&M settings NSC
- Fixed : below zero detection when taring in W&M modes
- Fixed : on coldstart recipe lines was allocated twice
- Fixed : Crash in DBASE calling system when timeout occurs
- Fixed : Misleading error message for PR1740 when no memory while downloading recipe
- Change : Default SW-Config Reports to NONE
- Fixed : CodeFault, when using recipe with textparameter on dosing FBs without tolerance
- Fixed : DSP_SELECT hangup, when using Delete key on PC-Keyboard
- Fixed : adjustment of ADC
- Fixed : Init Setpoint, Production, Consumption, Stock, when downloading recipe from PR1740
- first version of firmware for X5 devices
| | |