| | | |
Archive of all PC-Tools downloads This is the complete archive of PC-Tools available for download from Sartorius Mechatronics. It is provided as convenience for customers, who need to use specific versions of a given software. For new development we strongly recommend to use the current releases found on List of latest PC-Tools downloads. | | |
| | | |
| | |
| | | |
FlashIt!32 - Fixed : Problems with certain USB-Serial converters
- Fixed : Abnormal program termination on to long label list
- New : Added support for flashing labels into X3-PR5410
- New : Support for Combics Pro
- Fixed: Workaround for bug with EthernetFlash over PR1713/14
- New: Support for W&M-BIOS PR8901/10
- New: Support for flashing via ethernet
(Requires BIOS 3.10 or better) - New: Flashing blocks checked by MD5 signature
- New: Enhanced security when flashing BIOS
- Fixed: Flash of firmware for ethernet cards
- New: Support of X4 Devices
- Change: Now uses CHM as helpfile
- New: Check files shows a busy-bee and a message when done
- Fixed: Merging or Flashing projects exceeding the small memory unit of PR1730 corrupted firmware. (Introduced with 2.20.3)
- Fixed: open comport failed, when port from FlashIt!.ini didn't exist on PC
- Added: Allow load into ram (for internal use only)
- Change: Show Filename first in ListBoxes for ease of use
- New: Ability to read compressed hex files (*.hez)
- New: Additional W&M Authorization for trained personal
- Fixed: Wrong language was flashed, if Language-Name had special characters.
- Fixed: BCC Calculation for PR1730 Projects exceeding 512k FlashProm
(Projects merged with older Versions of FlashIt! should be merged once more) - New : Option "Check Files" removes files from comboboxes, which are not available any more
- New : Check for Flash-Size in PR1730 and issue an error, if project will not fit.
- Change : Allow flash of old BIOS without Hardware-Code in PR1713/00
- Change : Deny flash of X5-BIOS into Device with old bios
This version does not support X5 and is obsolete This version is obsolete | | |
| | | |
| | |
| | | |
PR1792Version: 2,4,3,0 Version: 2,4,2,0 Version: 2,4,0,0 - Fixed problem with database access on X4
- Added support for LMA200
- Updated error messages in help file
- Moved some error/warning messages to the debug class (only visible when debug option is on)
- Fixed issue 0001640 (alias file eror)
- X3, Ethernet Transmitter do not show database tag (issue: 0001440)
- The board number and device id is printed to the log file (issue:0000322)
- Fixed issue with missing init after disconnect from database (2.2.0.12)
- support for PR5220 (Ethernet Transmitter) (2.2.0.11)
- Fixed: Must restart OPC server after database structure read timeout (2.2.0.10)
- Fixed issue with missing init after disconnect from database
- Fixed: Reading weight values with database interface (AccessIt)
- Fixed: Downloading long database records (more than about 240 byte / record)
- Fixed: Access path is now ignored
- Fixed problem with normal user rights under XP
- New data type mb (byte) and mw (word) added
- Support for ProBatch+ added
- Aliases for item names are now possible.
- On some PC's there was a problem opening the configuration dialog. This was fixed.
- Support for X4 (5510) added
- You must have PR1792 version 2.0.0.75 installed. Replace the PR1792.exe and PR1792.map files with the new version included.
| | |
| | | |
| | |
| | | |
ConfigureIt! Supports PR5210 with LO number from 2611004000 Supports PR5210 with LO number from 2611004000 - Changed : User can now select the com port
Supports PR5210 with LO number from 2503003000 - New: Analog output adaption.
Supports PR5210 with LO number from 2503003000 - Fixed: ConfigureIt! is now running under japanese WindowsXP.
Supports PR5210 with LO number from 2311002000 Supports PR5210 with LO number from 2311002000 Supports PR5210 with LO number up to 2311002000 | | |
| | | |
| | |
| | | |
DongleMaintenanceTool | | |
| | | |
| | |
| | | |
pr1791v8100 | | |
| | | |
| | |
| | | |
Technical ReferenceExtract archive to an empty directory and use index.html as start document. | | |
| | | |
| | |
| | | |
| | | |
| | |
| | |
| © Sartorius Mechatronics, 2010 | | |
| | |
| | |
| | |